All News

Piab expands its new series of automotive suction cups with the addition of three new sub-families
Piab is proud to introduce a new series of automotive suction cups which address the applications within body shop and part assembly as well as low/medium speed press lines. These new cups add to a now complete program, all in all 22 new cups.

Automatic handling of boxes and interlayers for the production of security cards
With a single gripper consisting of four B75 silicon suction cups by Piab, Robotecnik designed and manufactured a palletising robot to handle efficiently the end-of-line operations of Banca d'Italia.

Absolute precision in the handling of thermoforms, with sealing rings, and their transport supports
System integrator Umbra Control chose Piab's Kenos® KCS gripper, in a special version with four suction cups, to accurately and efficiently handle Meccanotecnica Umbra's end-of-line pick and place operations for the production of seals for the automotive industry.

Safe conveying of instant milk granules with Piab’s piFLOW®p vacuum conveyor
Polmlek Raciaz, a Polish producer of various milk-based products faced a problem of breaking granules during the transfer of instant milk within its process. In Piab’s piFLOW®p vacuum conveyor they found the solution they were searching for. Equipped with an ejector with a high vacuum flow, they were able to adjust the speed to maintain the granules as planned.

piSAFE® launch - Full program now available
Piab's piSAFE® program is now supplemented with piSAFE® Vacuum Safety Valve and piSAFE® Vacuum Safety Valve Mini for centralized systems which marks the completion of the piSAFE® program.

Automated palletizing of sweet tea and juice from a cold room
While palletizing cartons is a regular automation application, doing so from a cold room that is regularly hosed with water to stay clean is a specific challenge. Motion Controls Robotics overcame these by using vacuum technology from Piab supplied by Neff Group Distributors.

Handling cheese blocks right with Piab’s vacuum technology
Packaging cheese blocks vacuum-wrapped in film represents a major challenge for process automation. With the help of Piab’s piGRIP® configurable suction cups and high-performance vacuum ejectors, the machine and plant manufacturer TGW Robotics GmbH has developed a gripper that ensures a stable process.

A great internal motivation driver
The X-Factor Interviews – Introducing the people behind the development of the MX Cup! Nicklas Holmgren – Content Creation Manager, Marketing Department – 5 years with Piab.

Tradichem uses Piab’s vacuum conveyor to miniaturize active pharma ingredients
Size matters – particularly in competitive markets such as pharma and nutraceuticals due to its direct result on costs. Tradichems patented Hipering® process begins right at the start of the process chain by miniaturizing the ingredients. Thanks to Piab’s piFLOW®p vacuum conveyor their patented process is continuously fed thus maintaining the required pressure level.

We do not copy others, we lead
The X-Factor Interviews – Introducing the people behind the development of the MX Cup! Lennart Ryberg – Global Product Manager, Vacuum Automation Division – 2.5 years with Piab

Mapping the gaps of customer needs
The X-Factor Interviews – Introducing the people behind the development of the MX Cup! Johnny Skagersjö – Senior Application Engineer in Automation div. and part of the System Engineering & Research team, with Piab since 2004

“Lagom” – not the best for something but just right for anything
The X-Factor Series – Introducing the people behind the development of the MX Suction Cup! Gustaf Wigren – Director Product Technology, Conceptual System Design, Research & Development (R&D), Automation Division – 13 years with Piab

Kora uses Piabs piFLOW®p vacuum conveyor for the efficient filling of superfoods
Fast and easy product changes, compliance with food and pharmaceutical standards, and high energy efficiency for sustainable resource conservation. For Kora the Piab vacuum conveyors are the perfect link between the process steps. Because they meet just these criteria.

The thinner the lip the better the grip
The X-Factor Series – Introducing the people behind the development of the MX Suction Cup Jonas Herrström – Senior Design Engineer, Conceptual System Design, Research & Development, Automation Division – 8 years with Piab

Piab conveys micro-additives for pet and farm animal food in Conberg solution
While micro-additives are an important part in today’s pet and farm animal food, their strongly varying amount per recipe poses a challenge in automating the transfer from dosage stations to the mixer. System integrator Conberg in Poland developed a suitable solution based on Piab’s piFLOW®f vacuum conveyor.

robominds calls Piab's new MX suction cup the "Super Cup"
According to robominds, the latest vacuum technology product from Piab has earned this nickname because it simply lifts anything - regardless of the material, geometry, or surface structure. And so, the all-rounder is exactly the suction cup that robominds has been missing for its picking solutions for eCommerce customers and manufacturers of complex products.

Piab is proud to announce the launch of the new piSAFE® program
Piab’s new piSAFE® program enables new benefits in applications where safety, flexibility, speed and performance are key.

New size to Bellows Flat Friction Suction Cup Family: BFFT80P-2
Piab expands its line of bellows flat friction suction cups to include a cup measuring 80 mm in diameter.

Automatic handling of cheese slice pouches of different formats at high process speeds
With the use of piGRIP® suction cups, certified for food contact, and COAX® vacuum generators, both Piab's products, CAMA Group has created a cutting-edge packaging system that allows to handle 280 pouches of cheese slices per minute.

The #1 item picker: Piab is proud to introduce the new MX suction cup family
The #1 Item picker. The MX suction cup family is exceptional for picking various objects primarily for the Logistics, Warehousing, E-commerce, and Re-cycling industries.

Automatic handling of pasta packs
With the use of a single Kenos® KVGL vacuum gripper by Piab, Selematic has created a state-of-the-art automatic packaging system, achieving a significant cost reduction and an important productivity increase when handling different formats and various layers of pasta.