Suggestions

Categories

Products

Content

News

170 articles
4/1/2021

Piab is proud to announce the launch of the new piSAFE® program

Piab’s new piSAFE® program enables new benefits in applications where safety, flexibility, speed and performance are key.

4/1/2021

New size to Bellows Flat Friction Suction Cup Family: BFFT80P-2

Piab expands its line of bellows flat friction suction cups to include a cup measuring 80 mm in diameter.

3/22/2021

Automatic handling of cheese slice pouches of different formats at high process speeds

With the use of piGRIP® suction cups, certified for food contact, and COAX® vacuum generators, both Piab's products, CAMA Group has created a cutting-edge packaging system that allows to handle 280 pouches of cheese slices per minute.

3/16/2021

The #1 item picker: Piab is proud to introduce the new MX suction cup family

The #1 Item picker. The MX suction cup family is exceptional for picking various objects primarily for the Logistics, Warehousing, E-commerce, and Recycling industries.

3/4/2021

Automatic handling of pasta packs

With the use of a single Kenos® KVGL vacuum gripper by Piab, Selematic has created a state-of-the-art automatic packaging system, achieving a significant cost reduction and an important productivity increase when handling different formats and various layers of pasta.

3/1/2021

Piab is evolving – A brand new customer-centric website launches today

With more than 650,000 users each year, Piab decided to up the ante on both the visual identity and the user experience of the new website. Through countless interviews, Piab created an even more customer-centric website which focuses on existing customers as well as exploring users.

2/3/2021

Piab is stepping up automation in the food industry, introducing a new vacuum-driven soft gripper

Cost effective solution for handling sensitive and difficult objects.

1/18/2021

The Changeover Champion

Change conveyed material in 10 minutes instead of 1 hour. piFLOW®p SMART offers six times faster changeover.

12/17/2020

It’s SMART to be safe with Piab’s next-gen

Piab’s piCOMPACT®23 SMART vacuum ejector includes optocouplers to ensure extra safe operation.

12/17/2020

Heavy-duty bag gripper for palletizing

Piab introduces the first-generation end-of-arm tools in 25 and 50kg payloads for palletizing a wide variety of products.

12/14/2020

Piab adds new 90 mm size to bellows suction cup configurator

Further broadening its already extensive application range, Piab extends its line of bellows suction cups to include cups measuring 90 mm in diameter.

12/10/2020

Piab adds new sizes to bellows suction cup line

Extra sizes, more functions in additional fittings, and the entire bellows suction cup line included in the online configurator.

11/30/2020

Piab enhances the piGRIP® bag lips (BGI): especially made for lifting sturdy and thin/delicate plastic bags

The BGI-Lip is great for picking both sturdy plastic bags and stand-up pouches filled with dry or wet food/substances. The BGI-2 lip, also gives excellent capabilities in picking thin/delicate plastic bags.

11/30/2020

Piab is proud to introduce the piSOFTGRIP® 50-2c

Piab once again extends the pi-SOFTGRIP® family with a new pinch gripper developed for the automation of the food/chocolate industry.

11/19/2020

Piab adds three new sizes to Rectangular Bellows family

Piab extends its program of Rectangular Bellows cups with two new cups featuring an extra bellow: the RBL20x45, RBL30x55, and a complete new “square” cup the RBL60x60.

Reduced assembly costs thanks to a piCOMPACT® all-in-one ejector
11/16/2020

Reduced assembly costs thanks to a piCOMPACT® all-in-one ejector

By changing over to our piCOMPACT® vacuum ejector, the customer reduced the installation effort thus saving time.

11/16/2020

New blog post: A gripping story

All stories have a beginning. The story of piSOFTGRIP® started with passion.

11/2/2020

Piab produces a new series of automotive suction cups

Piab is proud to introduce a new series of automotive suction cups which address the applications in the Body and Part assembly as well as in low/medium speed press lines.

11/2/2020

Piab introduces vacuum conveyor offer for the Additive Manufacturing industry

With extensive experience in material handling within the Pharmaceutical, Food and Chemicals industries, Piab is now extending its offer to the Additive Manufacturing industry.

11/1/2020

Piab adds COMPACT10E® to the compact pump program

The Piab compact pump program is now expanded with a new alternative, COMPACT10E®, to complement the smaller size 10mm pump program.

9/1/2020

ECU-15S piFLOW®p Smart

Piab continues the software development of the piFLOW®p SMART software platform, which focuses on ease of use and improved/added functionality

Compare products

0 item(s) added
Compare