Suggestions

Categories

Products

Content

News

95 articles
1/18/2021

The Changeover Champion

Change conveyed material in 10 minutes instead of 1 hour. piFLOW®p SMART offers six times faster changeover.

12/17/2020

It’s SMART to be safe with Piab’s next-gen

Piab’s piCOMPACT®23 SMART vacuum ejector includes optocouplers to ensure extra safe operation.

12/17/2020

Heavy-duty bag gripper for palletizing

Piab introduces the first-generation end-of-arm tools in 25 and 50kg payloads for palletizing a wide variety of products.

12/14/2020

Piab adds new 90 mm size to bellows suction cup configurator

Further broadening its already extensive application range, Piab extends its line of bellows suction cups to include cups measuring 90 mm in diameter.

12/10/2020

Piab adds new sizes to bellows suction cup line

Extra sizes, more functions in additional fittings, and the entire bellows suction cup line included in the online configurator.

11/30/2020

Piab enhances the piGRIP® bag lips (BGI): especially made for lifting sturdy and thin/delicate plastic bags

The BGI-Lip is great for picking both sturdy plastic bags and stand-up pouches filled with dry or wet food/substances. The BGI-2 lip, also gives excellent capabilities in picking thin/delicate plastic bags.

11/30/2020

Piab is proud to introduce the piSOFTGRIP® 50-2c

Piab once again extends the pi-SOFTGRIP® family with a new pinch gripper developed for the automation of the food/chocolate industry.

11/19/2020

Piab adds three new sizes to Rectangular Bellows family

Piab extends its program of Rectangular Bellows cups with two new cups featuring an extra bellow: the RBL20x45, RBL30x55, and a complete new “square” cup the RBL60x60.

11/2/2020

Piab produces a new series of automotive suction cups

Piab is proud to introduce a new series of automotive suction cups which address the applications in the Body and Part assembly as well as in low/medium speed press lines.

11/2/2020

Piab introduces vacuum conveyor offer for the Additive Manufacturing industry

With extensive experience in material handling within the Pharmaceutical, Food and Chemicals industries, Piab is now extending its offer to the Additive Manufacturing industry.

11/1/2020

Piab adds COMPACT10E® to the compact pump program

The Piab compact pump program is now expanded with a new alternative, COMPACT10E®, to complement the smaller size 10mm pump program.

9/1/2020

ECU-15S piFLOW®p Smart

Piab continues the software development of the piFLOW®p SMART software platform, which focuses on ease of use and improved/added functionality

9/1/2020

Piab extends the piSOFTGRIP® program with the piSOFTGRIP® 30-3

Piab is proud to introduce a new smaller size of the soft gripping tool piSOFTGRIP®, developed especially for the food/chocolate industry.

9/1/2020

ECU-15- piFLOW® Electrical controller

The new software platform both for ECU-15 and ECU-15S can easily be upgraded with new software releases, adding new functionality in the future.

6/30/2020

Piab adds new size to Bellows Flat Friction Cup Family

Further broadening its already extensive application range, Piab expands its line of bellows flat friction cups to include a cup measuring 60 mm in diameter.

6/1/2020

Kenos® KVG60 gripper system now available to configure with Piab suction cups

With Piab’s new configurator tool, it is easy to design a KVG60 gripper system equipped with vacuum generation as well as Piab’s suction cups and flow control valves.

5/31/2020

piCOBOT® is available with a plug and play configuration for the Fanuc CR4/CR7 robots

Through the user-friendly online configuration tool, Piab’s customers can now make the choice to have the piCOBOT® specified to the Fanuc robots CR4 & CR7.

5/5/2020

Piab’s Chip ejector eases breathing for COVID-19 patients

A large medtech manufacturer has increased its production of bronchial secretion aspirators. Piab has followed suit and can thus deliver its Chip ejector in large quantities at short notice.

4/27/2020

Three new bag gripping products ready for robots

Piab offers a wide range of End Of Arm Tooling (EOAT) for industrial robotic palletizing and de-palletizing operations, which are now on our website.

3/31/2020

Introducing the piFLOW®i/f 28L vacuum conveyor

Piab is extending the piFLOW®i/f family range with a new vacuum conveyor that allows for larger batch volume.

3/1/2020

Introducing the mid-range piFLOW®fc vacuum conveyor

Chocolates, cookies, crisps and coffee but also certain chemicals – the piFLOW®fc vacuum conveyor handles all.

Compare products

0 item(s) added
Compare