News

The dm distribution center relies on Piab suction cups
dm is currently the largest drugstore in Europe. At their distribution center a large part of the pallets is depalletized with...

With piSOFTGRIP® 100-4, Piab is launching the largest gripper of this series
Piab is proud to introduce the new and largest soft gripper developed especially with food industry...

A partnership between Höganäs and Piab is set to make Additive Manufacturing more sustainable and efficient
Höganäs and Piab have formed a partnership to leverage their respective areas of expertise with the goal of advancing...

Elevating the learning experience
To better facilitate a high-performing learning environment for our customers and partners, we at Piab is now launching...

Safe automatic handling of glass sheets with Piab’s vacuum technology
Forvet SpA has created end-of-arm tools that allow handling glass sheets of different sizes...

Piab introduces piFLOW®am
The piFLOW®am is a small vacuum conveyor designed based on requirements from OEMs within the Additive...

Ergonomic hazards in the Food industry and how to eliminate them
The food production line is a hazardous one. Therefore, it is extremely important to avoid...

Now available – the gripper for automated handling of six-packs
With Piab’s new gripper, six-packs with cardboard wrapping can be handled automatically, gently and...

Respiratory hazards in the Food industry and how to eliminate them
With allergies, asthma, and other conditions becoming more frequent, processors need to implement changes...

With Piab’s area gripper, the handling of furniture parts is child's play
The machine builder GO GmbH were looking for an “all-in-one” gripper solution that can be used to stack both loose and packaged furniture parts on and off pallets, as well as the pallets themselves. The solution was...

Delivering clean sugar with Piab’s piFLOW®p vacuum conveyor
To improve product quality and prevent losses India’s leading manufacturer M. B. Sugar trusts...

At Nipro the piCOMPACT® provides the vacuum performance needed in production of pharma packaging made of glass
With 32,500 cycles per day, 24 hours a day, seven days a week, this application is one of the those with the highest number of...

JAM Automation moves 550lb heavy profiles with Piab’s Kenos® grippers
To automaticaly remove extruded aluminium profiles from cassettes in high-bay warehouses, JAM Automation created...

Automating powder handling in Additive Manufacturing
Automating metal powder handling is key to establish the Additive Manufacturing technology as a standard process. Piab’s vacuum conveying powder...

Automatic handling of porcelain stoneware slabs and related sub-formats
Thanks to Piab's Kenos® KVG area vacuum gripper, an extreme variability of sizes and surfaces can be managed, using just a single gripper. This allowed...

Piab extends the Kenos® Sack Gripper program
The highly reliable Kenos® KSG gripper is now extended with a new smaller size, sealing ring and can now also be configured with...

Kenos® Reverse valves program is extended
The KRV reverse valve controls the air flow and is typically used in external vacuum generator systems. Robust and reliable, KRV valves are offered in models for...

High flexibility and safe gripping in a cosmetic application with Piab's cobot gripper
Effedi Automation chose the piCOBOT® gripper, COAX® vacuum technology and BX suction cups by Piab to handle the palletizing operations of a...

Piab extends the VGS™ product range with VGS™4005
The VGS™4005 is geared to cater for mid-range applications where less vacuum depth is needed. The vacuum gripper ejectors are robust, easy to use and designed to...