News

Industrial Bakery Austerschmidt in Germany automates handling of seeds with Piab’s vacuum conveyors
Employee relief and careful use of resources prompted the industrial bakery Austerschmidt in Germany to switch the handling of seeds from a manual to an automated process. In piFLOW®f vacuum conveyors, they found the critical tools.

With Piab's gripper, Best Handling Technology improves the ergonomics of its customer at 32 workstations
Healthy, satisfied employees, increased efficiency, flexibility, and sustainability - regardless of the industry, the reasons are always the same that give cause to a higher degree of automation in handling tasks. German Best Handling Technology was able to achieve all of this for its customer, a leading logistics service provider, with a suction cup equipped Kenos® area gripper.

DCL realizes flexible automation solution with Piab’s piCOBOT® gripper on an UR 10e robot
Looking for a flexible, easy to integrate, plug-and-play solution to handle picking and packing of items into boxes in their fulfilment center DCL Logistics based in Fremont, CA, resorted to an UR 10e robot combined with Piab’s piCOBOT® vacuum gripper.

Conveying made easy with Piab’s piFLOW®p SMART Conveying Cycle Optimizer (CCO)
Wouldn’t conveying more material at the same time, with less requirements on operator skills and saving on energy costs sound great? If so, check out Piab’s newest edition to its premium conveyor series.

Piab launches the Vacuplus ejector series for low to mid-range applications
As a part of our ambition to expand our global portfolio, we at Piab are thrilled to present the launch of our Vacuplus ejectors, geared to cater for low to mid-range applications that cannot compromise on ejector performance.

Piab expands its new series of automotive suction cups with the addition of three new sub-families
Piab is proud to introduce a new series of automotive suction cups which address the applications within body shop and part assembly as well as low/medium speed press lines. These new cups add to a now complete program, all in all 22 new cups.

Automatic handling of boxes and interlayers for the production of security cards
With a single gripper consisting of four B75 silicone suction cups by Piab, Robotecnik designed and manufactured a palletizing robot to handle efficiently the end-of-line operations of Banca d'Italia.

Absolute precision in the handling of thermoforms, with sealing rings, and their transport supports
System integrator Umbra Control chose Piab's Kenos® KCS gripper, in a special version with four suction cups, to accurately and efficiently handle Meccanotecnica Umbra's end-of-line pick and place operations for the production of seals for the automotive industry.

Safe conveying of instant milk granules with Piab’s piFLOW®p vacuum conveyor
Polmlek Raciaz, a Polish producer of various milk-based products faced a problem of breaking granules during the transfer of instant milk within its process. In Piab’s piFLOW®p vacuum conveyor they found the solution they were searching for. Equipped with an ejector with a high vacuum flow, they were able to adjust the speed to maintain the granules as planned.

piSAFE® launch - Full program now available
Piab's piSAFE® program is now supplemented with piSAFE® Vacuum Safety Valve and piSAFE® Vacuum Safety Valve Mini for centralized systems which marks the completion of the piSAFE® program.

Automated palletizing of sweet tea and juice from a cold room
While palletizing cartons is a regular automation application, doing so from a cold room that is regularly hosed with water to stay clean is a specific challenge. Motion Controls Robotics overcame these by using vacuum technology from Piab supplied by Neff Group Distributors.

Handling cheese blocks right with Piab’s vacuum technology
Packaging cheese blocks vacuum-wrapped in film represents a major challenge for process automation. With the help of Piab’s piGRIP® configurable suction cups and high-performance vacuum ejectors, the machine and plant manufacturer TGW Robotics GmbH has developed a gripper that ensures a stable process.

A great internal motivation driver
The X-Factor Interviews – Introducing the people behind the development of the MX Cup! Nicklas Holmgren – Content Creation Manager, Marketing Department – 5 years with Piab.

Tradichem uses Piab’s vacuum conveyor to miniaturize active pharma ingredients
Size matters – particularly in competitive markets such as pharma and nutraceuticals due to its direct result on costs. Tradichems patented Hipering® process begins right at the start of the process chain by miniaturizing the ingredients. Thanks to Piab’s piFLOW®p vacuum conveyor their patented process is continuously fed thus maintaining the required pressure level.

We do not copy others, we lead
The X-Factor Interviews – Introducing the people behind the development of the MX Cup! Lennart Ryberg – Global Product Manager, Vacuum Automation Division – 2.5 years with Piab.

Mapping the gaps of customer needs
The X-Factor Interviews – Introducing the people behind the development of the MX Cup! Johnny Skagersjö – Senior Application Engineer in Automation div. and part of the System Engineering & Research team, with Piab since 2004

“Lagom” – not the best for something but just right for anything
The X-Factor Series – Introducing the people behind the development of the MX Suction Cup! Gustaf Wigren – Director Product Technology, Conceptual System Design, Research & Development (R&D), Automation Division – 13 years with Piab

Kora uses Piabs piFLOW®p vacuum conveyor for the efficient filling of superfoods
Fast and easy product changes, compliance with food and pharmaceutical standards, and high energy efficiency for sustainable resource conservation. For Kora the Piab vacuum conveyors are the perfect link between the process steps. Because they meet just these criteria.

The thinner the lip the better the grip
The X-Factor Series – Introducing the people behind the development of the MX Suction Cup Jonas Herrström – Senior Design Engineer, Conceptual System Design, Research & Development, Automation Division – 8 years with Piab

Piab conveys micro-additives for pet and farm animal food in Conberg solution
While micro-additives are an important part in today’s pet and farm animal food, their strongly varying amount per recipe poses a challenge in automating the transfer from dosage stations to the mixer. System integrator Conberg in Poland developed a suitable solution based on Piab’s piFLOW®f vacuum conveyor.

robominds calls Piab's new MX suction cup the "Super Cup"
According to robominds, the latest vacuum technology product from Piab has earned this nickname because it simply lifts anything - regardless of the material, geometry, or surface structure. And so, the all-rounder is exactly the suction cup that robominds has been missing for its picking solutions for eCommerce customers and manufacturers of complex products.