News

Quick to market with new canned products thanks to efficient palletizing solutions from Piab
With Piab‘s Kenos® area gripper, the duration of the palletizing process of food and beverage cans is significantly...

With piSOFTGRIP® 100-4, Piab is launching the largest gripper of this series
Piab is proud to introduce the new and largest soft gripper developed especially with food industry...

A partnership between Höganäs and Piab is set to make Additive Manufacturing more sustainable and efficient
Höganäs and Piab have formed a partnership to leverage their respective areas of expertise with the goal of advancing...

Elevating the learning experience
To better facilitate a high-performing learning environment for our customers and partners, we at Piab is now launching...

Piab introduces piFLOW®am
The piFLOW®am is a small vacuum conveyor designed based on requirements from OEMs within the Additive...

Now available – the gripper for automated handling of six-packs
With Piab’s new gripper, six-packs with cardboard wrapping can be handled automatically, gently and...

Automating powder handling in Additive Manufacturing
Automating metal powder handling is key to establish the Additive Manufacturing technology as a standard process. Piab’s vacuum conveying powder...

Piab extends the Kenos® Sack Gripper program
The highly reliable Kenos® KSG gripper is now extended with a new smaller size, sealing ring and can now also be configured with...

Kenos® Reverse valves program is extended
The KRV reverse valve controls the air flow and is typically used in external vacuum generator systems. Robust and reliable, KRV valves are offered in models for...

Piab extends the VGS™ product range with VGS™4005
The VGS™4005 is geared to cater for mid-range applications where less vacuum depth is needed. The vacuum gripper ejectors are robust, easy to use and designed to...

Conveying made easy with Piab’s piFLOW®p SMART Conveying Cycle Optimizer (CCO)
Wouldn’t conveying more material at the same time, with less requirements on operator skills and saving on energy costs sound great? If so, check out Piab’s newest edition to its premium conveyor series.

Piab launches the Vacuplus ejector series for low to mid-range applications
As a part of our ambition to expand our global portfolio, we at Piab are thrilled to present the launch of our Vacuplus ejectors, geared to cater for low to mid-range applications that cannot compromise on ejector performance.

Piab expands its new series of automotive suction cups with the addition of three new sub-families
Piab is proud to introduce a new series of automotive suction cups which address the applications within body shop and part assembly as well as low/medium speed press lines. These new cups add to a now complete program, all in all 22 new cups.

piSAFE® launch - Full program now available
Piab's piSAFE® program is now supplemented with piSAFE® Vacuum Safety Valve and piSAFE® Vacuum Safety Valve Mini for centralized systems which marks the completion of the piSAFE® program.

Piab is proud to announce the launch of the new piSAFE® program
Piab’s new piSAFE® program enables new benefits in applications where safety, flexibility, speed and performance are key.

New size to Bellows Flat Friction Suction Cup Family: BFFT80P-2
Piab expands its line of bellows flat friction suction cups to include a cup measuring 80 mm in diameter.

The #1 item picker: Piab is proud to introduce the new MX suction cup family
The #1 Item picker. The MX suction cup family is exceptional for picking various objects primarily for the Logistics, Warehousing, E-commerce, and Recycling industries.

Piab is evolving – A brand new customer-centric website launches today
With more than 650,000 users each year, Piab decided to up the ante on both the visual identity and the user experience of the new website. Through countless interviews, Piab created an even more customer-centric website which focuses on existing customers as well as exploring users.

Piab is stepping up automation in the food industry, introducing a new vacuum-driven soft gripper
Cost effective solution for handling sensitive and difficult objects.