- Nyheter
- Help for strawberry shortcake lovers
Help for strawberry shortcake lovers

With Piab's combination of conveying, gripping and lifting tools, strawberry shortcakes can be baked quickly and safely packed for transport.
If you love strawberry shortcake, you will surely be interested in how it gets freshly baked and well packaged in your freezer so that you always have a piece ready.
With the piFLOW®p SMART, flour, sugar and all other powdered ingredients for the cake base are added directly to the mixer in the correct mixing ratio. Thanks to the auto-tuning function, the change from one ingredient to the other can be done in just 10 minutes, six times faster than before manually. Accordingly, further cake bases can be produced more quickly.
To avoid anyone in the bakery injuring their back when unloading the flour and sugar sacks into the feed station of the piFLOW®p SMART, there is the piLIFT® SMART. Piab’s vacuum lifter makes handling 40 kg sacks child's play. It counts and weighs how much powder has been emptied into the removal station. This allows the employee to concentrate on the preparation of the covering.
Once the cake base is baked, it can be placed directly on a cardboard mat where Piab’s latest coup, the Mini Cobot Gripper, picks up and places. At just 270 grams, the Mini Cobot Gripper is a featherweight among the Cobot grippers. It can lift up to five kilograms and has a height of only 28 millimeters.
Thanks to the piSOFTGRIP®, strawberries can be automatically placed in the cake base with a cobot or industrial robot. It handles the sensitive fruits gently and yet safely with its combination of vacuum chamber and fingers.
Once the strawberry shortcake has been shrink-wrapped and packed in boxes, Piab’s usual handling tools such as piGRIP® suction cups and the powerful COAX®-based vacuum ejectors can be used to place the boxes in the outer packaging and stack them on a pallet.
About Piab
Piab provides smart solutions for the automated world, helping thousands of end users and machine producers in e-commerce logistics, food, pharma, automotive and other manufacturing industries to improve energy-efficiency, productivity and working environments. With more than 500 employees and SEK 1,2 bn in sales 2018, Piab is a global organization, serving customers in almost 70 countries from a network of subsidiaries and distributors. By leveraging the ongoing technological development in automation and robotics, and targeting high-growth segments and geographies, Piab's vision is to become the global leader in gripping and moving solutions.
For more information please contact:
Andrea Bodenhagen, Global Ownership Content Manager
Tel.: +49 (0) 6033-7960-107
Email: andrea.bodenhagen@piab.com