- Industries
- Food & Beverage
- Nutraceuticals
- Fiber drum and barrel pick-up
Nutraceuticals
Fiber drum and barrel pick-up
When working with hazardous materials, it is crucial to minimize employee interaction as much as possible. Emptying barrels and drums is not only manually intensive but employees are often exposed to the dangerous content.
Piab is the only market provider offering a vacuum conveyor that not only replaces the manual work with an automated barrel pick up, but also an enclosed system which reduces the risk of particle exposure to employees.