- 새소식
- Selected Joulin grippers now sold under the Kenos® brand
Selected Joulin grippers now sold under the Kenos® brand

End of May, Piab acquired Joulin, a global leader of vacuum gripping solutions. Now, Piab has integrated three of Joulin's gripper ranges into its Kenos® portfolio, while the solutions for the heavy duty industries continue to be marketed under the Joulin brand, who’s experts further support these industries in defining the best system for each individual customer.
As the market for material handling solutions is growing rapidly, Joulin has a perfect strategic fit to the Piab business. Through the acquisition, Piab is evolving automation further by strengthening our position as a world leading automation company in our core industries and applications as well as taking a significant step into the raw wood industry, building on Joulin's 60 years of experience.
To further reinforce and expand the solutions business in heavy duty applications and the wood industry, these solutions consisting of large grippers and gantry cranes will continue to be marketed under the Joulin brand. The industry known experts will remain to design and build solutions matching individual customer needs and provide their top service.
At the same time the selected gripper ranges developed by Joulin, including the MiniGrip, the FlexiGrip and the Safe&Light are integrated into the Kenos® brand, which perfectly complements the existing Piab portfolio and further strengthens the support different needs of the customers.
The Kenos® MiniGrip (KMG) is suitable for the FMCG, food & beverage and automotive industries. It is a foam gripper that can be adapted to tight clearance applications in an End-of-Arm Tooling (EOAT). Its foam surface offers the versatility to pick a variety of different objects without adjustment. In case of uneven layer heights KMG can be equipped with level compensators without needing to change the mounting device. Find out more about it by clicking here!
The Kenos® FlexiGrip (KFG) is suitable for food & beverage, automotive and construction industries. It is a vacuum foam gripper that can be used as a single gripper on robots as well as on cobots, or combined into an EOAT for use with industrial robots. With its foam surface it offers the flexibility to pick a variety of different products without adjustment. Its modular design provides the flexibility for fast and easy set-up in case of product changes as well as simple integration in to existing equipment. Find out more about it by clicking here!
The Kenos® Safe&Light (KSL) is suitable for use in applications such as packaging, warehousing, end-of-line production. Thanks to its special design of a carbon fiber structure holding a foam made body, it is extremely lightweight allowing to make maximum use of the robot or cobot payload. It is a robust and simple solution for a broad range of purposes, particularly for palletizing applications in rugged and dusty environments. Find out more about it by clicking here!
As a vacuum technology leader Piab offers a wide range of solutions for various industries and applications, from suction cups and pumps to full EOAT and custom solutions. Whatever the needs and requirements on the application are Piab’s experts support all customers in the right selection of gripping tools and act as reliable partner from the beginning and beyond.
More information
Luba Biber, Global Marketing Manager, Vacuum Automation Division
+49 (0) 6033 7960 0
Piab Vakuum GmbH, Otto-Hahn-Str. 14, 35510 Butzbach, Germany
www.piab.com
About Piab
At Piab we evolve automation, creating sustainable solutions for a safer and more efficient workplace in an automated world. We provide gripping skills to robots, intelligent flow to materials, and lifting power to humans. We want to improve today’s world for the better. This ambition is embedded into everything we do. It is in every idea, every interaction, every product, and solution we provide. Our customers are in just every sector, including the food & beverage, automotive, packaging, logistics & warehousing, e-commerce, electronics, chemicals, and pharmaceutical industries, and general manufacturing.
Piab´s vision is an automated world where no resources are wasted, and no humans are injured.
With sales of c. 1.9 BSEK, more than 1000 employees and 4 divisions, Piab is a global organisation, serving customers in more than 100 countries from a network of subsidiaries and distributors.
Evolving ourselves.
Evolving you.
Evolving automation.