Nowości

piCOBOT® dostępny z konfiguracją typu „plug and play” dla robotów Fanuc CR4/CR7
Dzięki wygodnemu w obsłudze narzędziu konfiguracyjnemu dostępnemu online klienci firmy Piab mogą teraz dobrać specyfikację zestawu piCOBOT® do robotów Fanuc CR4 & CR7.

System chwytaków próżniowych Kenos® KVG60 można teraz skonfigurować z przyssawkami Piab
Za pomocą nowego konfiguratora firmy Piab można łatwo i szybko zaprojektować system chwytaków KVG60 wyposażony w technologię generowania podciśnienia oraz przyssawki Piab i zawory sterujące przepływem.

Visors protecting people against COVID-19 from Somtech are now handled with Piab components
The fast delivery of gripping components from Piab allows Somtech to produce 56,000 visors a week with immediate effect.

Piab’s Chip ejector eases breathing for COVID-19 patients
A large medtech manufacturer has increased its production of bronchial secretion aspirators. Piab has followed suit and can thus deliver its Chip ejector in large quantities at short notice.

Trzy nowe chwytacze worków do robotów
Firma Piab oferuje szeroką gamę narzędzi krańcowych do ramion robotów (EOAT, End Of Arm Tooling) do przemysłowych operacji paletyzacji i depaletyzacji wykonywanych za pomocą robotów. Narzędzia te są już dostępne w naszej witrynie internetowej.

Introducing the piFLOW®i/f 28L vacuum conveyor
Piab is extending the piFLOW®i/f family range with a new vacuum conveyor that allows for larger batch volume.

Introducing the mid-range piFLOW®fc vacuum conveyor
Chocolates, cookies, crisps and coffee but also certain chemicals – the piFLOW®fc vacuum conveyor handles all.

Piab awarded ”Employer of the Year”!
We are incredibly proud to be awarded one of the Employers of the Year within the Construction and Manufacturing industries.

Piab’s hybrid bag gripper increased productivity by 33%
Sapho can now palletize 9 bags per minute instead of 6 with the old system and the process runs smoothly without damaging the road salt bags.

With Piab’s bag grippers, Sapho increases its pace
With Piab's hybrid bag gripper, Sapho was able to significantly increase their cycle times in order to be optimally prepared for the winter business for road salt.

Digitizing vacuum generation enables predictive maintenance of robotic handling systems
Piab has upgraded its flagship product – the piCOMPACT® vacuum ejector series – to support Industry 4.0 functionality.

New blog post: A gripping story
All stories have a beginning. The story of piSOFTGRIP® started with passion.

It’s down to collaboration
Cobots enable greater collaboration between humans and machines. In order to do so, cobots need cleverly designed end-of-arm tools (EOATs).
Piab Group has through Piab AB signed an agreement to acquire the business of PIVAC Syd AB
Pivac Syd AB is one of Piab’s current distributors of innovative vacuum solutions in Sweden.

Making piCOBOT® even more collaborative
Piab’s clever end-of-arm (EOAT) vacuum tool piCOBOT® extends its reach into the cobot market - now configurable for any cobot.
Piab Group has through Piab AB signed an agreement to acquire the businesses of Belker Vakuumteknik AB and PI-VAC AB
Belker Vakuumteknik AB and PI-VAC AB are two of Piab’s most important and long serving distributors in Sweden.

Is it safe or even possible to transport dry materials in high heels?
Safety should always come first when you work in manufacturing. Does that mean that you should stay away from manufacturing industries if you love wearing high heels?

Mistrz zmian transportu próżniowego Piab
Uczenie maszynowe w nowym, unikalnym systemie piFLOW®p SMART przenosi transport próżniowy na nowy poziom.

Nowoczesne rozwiązania EOAT dla branży tworzyw sztucznych
Chwytaki próżniowe firmy Piab zostały specjalnie zaprojektowane z myślą o wyjmowaniu plastikowych elementów z form.

Firma Piab dodaje nowy rozmiar 65 mm do linii przyssawek mieszków
Firma Piab poszerzając i tak już szeroki zakres zastosowań, rozszerza linię przyssawek mieszkowych o przyssawki o średnicy 65 mm.

Mistrz zmian
Zmiana przenoszonego materiału w ciągu 10 minut zamiast 1 godziny. piFLOW®p SMART oferuje sześciokrotnie szybszą zmianę.