- News
- Piab adds new 65 mm size to bellows suction cup line
Piab adds new 65 mm size to bellows suction cup line

Extra sizes, more functions in additional fittings, and the entire bellows suction cup line included in the configurator.
Taby, Sweden – Piab is extending its generic line of bellows suction cups to include cups measuring 65 mm in diameter, further broadening its already extensive application range. The new cup size is the last of four new sizes added to the popular bellows suction cup line. Cups measuring 13, 26, and 90 mm have recently been introduced.
“We decided to plug a few gaps in our size line-up for bellows suction cups. The extension will enable us to offer our customers an expanded range of options perfectly suited to their respective applications,” says Josef Karbassi, Vice President for Piab’s Automation Division.
“In addition to this, we have added extra fittings for several of our existing bellows cups, and the entire bellows suction cup line has been included in our popular customer online configurator,” he continues.
The wider range of fittings now available for a selected number of Piab’s bellows suction cups offers further optional functions, such as specialised flow-control valves and filters. To assist selection and tailor-made solutions, these fittings and the full range of standard bellows suction cups (B5 to B150) are featured in Piab’s configuration tool, available on the company’s website.
The new bellows cups are available in four different materials - nitrile rubber (NBR), the non-marking HNBR, and two grades of silicone. The standard grade silicone is used for bellows cups widely used within the plastics and packaging industries, and the alternative food-grade silicone is offered for cups used by industries that need to adhere to hygiene standards set by the US (FDA 21CFR177.2600) and/or the EU (EU 1935/2004).
“The very high and consistent quality of our bellows suction cups stems from the fact that we use certified and high-quality materials. Our customers appreciate that they can trust that each new batch of cups they order will be the same as the last one they had from us,” says Josef Karbassi.
About Piab
Piab provides smart solutions for the automated world, helping thousands of end users and machine producers in e-commerce logistics, food, pharma, automotive and other manufacturing industries to improve energy-efficiency, productivity and working environments. With almost 500 employees and SEK 1.2 bn in sales 2018, Piab is a global organization, serving customers in almost 70 countries from a network of subsidiaries and distributors. By leveraging the ongoing technological development in automation and robotics, and targeting high-growth segments and geographies, Piab’s vision is to become the global leader in gripping and moving solutions.
More information
Kajsa Blixth, Vice President Marketing and Communications Manager
Tel: +46 (0) 8 630 25 00
E-mail: kajsa.blixth@piab.com